Commercial cleaning is essential, especially when considering how it can impact our health associated with inhaling dust indoors. When commercial cleaning companies and janitorial services choose the right tools, they aren’t simply trying to make things look good — they’re cleaning for health so you can breathe air with fewer dust and debris contaminants.
 

Capturing and containing dust and debris


 

Many backpack vacuums are engineered to rely on suction for picking up debris rather than a beater bar like a traditional, upright vacuum. According to a study performed by Quality Environmental Solutions & Technologies, Inc. (QuES&T), backpack vacuums are more efficient than uprights at capturing and containing dust and debris.

The powerful suction of a backpack vacuum compared to a traditional upright vacuum helps ensure dirt and debris are collected without stirring up significant dust. And with advanced filtration systems, particles that can be harmful to your health are put where they belong — in the vacuum.
 

Enjoying cleaner indoor air
 

Microscopic dust can be harmful to our health and trigger asthma and allergies. With approximately 13.8 million school days and 14.2 million workdays missed each year due to asthma, it’s easy to see how cleaner air with less dust and debris can make a difference.

Backpack vacuums with such features as multiple layers of filtration are an excellent tool for capturing dust to help with cleaning for health. When you pair powerful suction with extendable wands and high dusting kits, a deeper clean is within reach. This makes tackling those ceiling vents, ducts and high corners easier.

Many commercial janitorial services also use backpack vacuums to make challenging cleaning scenarios easier to navigate. Since the body of a backpack vacuum is carried on a user’s back, they have more freedom to move than with upright vacuums. Additionally, users can efficiently work around desks, kiosks and other stationary objects with backpack vacuums.

With powerful suction and the versatility to reach high and low places, backpack vacuums are an excellent tool for capturing and containing dust and debris in a multitude of places.
 

Achieving a green clean
 

Leadership in Energy and Environmental Design, or LEED, is a leading green building certification. Each year, more businesses seek LEED certification to demonstrate their commitment to green building standards and the health of their patrons and the environment.

While there are many requirements for such recognition, indoor air quality (IAQ) is at the top of the list. Commercial cleaning companies that serve LEED-certified clients must use vacuums that meet specific vac standards to maintain LEED certification.

Fortunately, many backpack vacuums check the LEED box. If you’re serious about cleaning for health and maintaining a LEED certification, make sure your backpack vacuums meet the following LEED requirements:

  • must be certified by the Carpet and Rug Institute Seal of Approval/Green Label 1
  • operate with a maximum sound level of 70 dBA or less in accordance with ISO 11201 2
     

Recognizing the best backpack vacuums in commercial cleaning
 

For more than 30 years, ProTeam has been a leader in commercial cleaning innovation. Notably, the same study conducted by QuES&T, found ProTeam backpack vacuums remove 43% more soil from carpets than commercial uprights and 30% more than canister vacuums in just five passes.

And ProTeam has used its 3+ decades of experience and research to develop one of the most advanced vacuum filtration systems on the market. With so many models that meet LEED requirements, ProTeam is an easy choice.

To learn more about how ProTeam can help you create cleaner and healthier environments, click here.

Please enable JavaScript to use this website.